Hi
Could you please help me to open a session to SE050-E over I2C bus? This is as far as I could get with documentation and examples available:
int
main(int argc, char **argv)
{
sss_session_t sesh;
SE_Connect_Ctx_t connectCtx = {0};
connectCtx.skip_select_applet = 1;
connectCtx.sessionResume = 1;
connectCtx.auth.authType = kSSS_AuthType_None;
connectCtx.portName = portName;
connectCtx.connType = kType_SE_Conn_Type_T1oI2C;
status = sss_session_open(&sesh, kType_SSS_SE_SE05x, 0, kSSS_ConnectionType_Plain, void *connectionData)
And I am stuck with portName. I assume it should be something along the line of "/dev/i2c-1:0x48" but could you confirm that?
已解决! 转到解答。
Hi @psvz ,
The port name can be fetched from the environment variable of "EX_SSS_BOOT_SSS_PORT", you may refer to ex_sss_boot_connectstring() for details, but for T1oI2c case, you may define it as Null.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @psvz ,
The port name can be fetched from the environment variable of "EX_SSS_BOOT_SSS_PORT", you may refer to ex_sss_boot_connectstring() for details, but for T1oI2c case, you may define it as Null.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------