JCOP 4 tools install is defeating me

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JCOP 4 tools install is defeating me

6,234 Views
msjcard
Contributor III

I'm finally getting around to installing JCOP tools (V5.20.1.4) and Eclipse - mainly because I've been unable to use jdb (from JDK11) with the JCOP4 simulator and wanted to see if perhaps Eclipse and the plugin might work.

I downloaded and installed the most recent version of Eclipse  (2020-09), and successfully installed and activated the JCOP 4 plugin.

Trying to build the template as a project (which happens automatically after the completing the project creation of an applet) gets me:

Errors occurred during the build.
Errors running builder 'Cap File Verifier' on project 'mfgapplet'.
begin 0, end -1, length 1

From:

java.lang.StringIndexOutOfBoundsException: begin 0, end -1, length 1
at java.base/java.lang.String.checkBoundsBeginEnd(String.java:3319)
at java.base/java.lang.String.substring(String.java:1874)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.checkJavaVersionCompatibilityForCapFileVerifier(VerifierBuilder.java:406)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.build(VerifierBuilder.java:72)
at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:832)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
at org.eclipse.ui.actions.BuildAction$1.runInWorkspace(BuildAction.java:291)
at org.eclipse.core.internal.resources.InternalWorkspaceJob.run(InternalWorkspaceJob.java:42)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

Trying this again with an applet that compiles through ANT and the JCDK tools still results in the above.

I've also tried this with a couple of earlier versions of Eclipse.  On one I get the same error, on the even earlier one (Luna) I can't even get an error message and no build appears to happen.

The is Windows 10 64bit, latest build, with Java 11 running Eclipse.   Or for that matter Java 8.  I'm specifying JC3.0.5 and no GP or JCOP libraries.  This happens on both machines I have access to, one a machine mostly fresh out of the box so few possibilities of other things interfering.

Any help would be appreciated.  Mike

0 Kudos
Reply
4 Replies

5,590 Views
Tobias_Ehrlich
Contributor I

The thread is a bit older, but I have basically the same problem, unfortunately, the above solution does not work for me. However I can provide some more information about.

Next to the eclipse Kepler version I have used

eclipse: 4.21.0.I20210906-0500 -- 2021-09 (4.21.0)

OS=linux, ARCH=x86_64, WS=gtk, NL=de_DE

NXP JCOP Tools 5.34.1.1 and profile JCOP Simulator 5.2-R2.02.1-0.21-1.3-1.5.148-profileU

Oracle JC tools 305u1/305u4 310b5

Java: Oracle jdk16.0.2, jdk180_202  and I also tried openJDK11

As Mentioned above the error message is:

Errors running builder 'Cap File Verifier' on project 'csp.demo'.

With the stack trace:

java.lang.StringIndexOutOfBoundsException: begin 0, end -1, length 1
at java.base/java.lang.String.checkBoundsBeginEnd(String.java:3751)
at java.base/java.lang.String.substring(String.java:1907)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.checkJavaVersionCompatibilityForCapFileVerifier(VerifierBuilder.java:406)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.build(VerifierBuilder.java:72)
at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:853)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:232)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:281)
at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:334)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:337)
at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:389)
at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:410)
at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:516)
at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:413)
at org.eclipse.ui.actions.BuildAction$1.runInWorkspace(BuildAction.java:291)
at org.eclipse.core.internal.resources.InternalWorkspaceJob.run(InternalWorkspaceJob.java:42)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

In eclipse Kepler the error message is more precise and says that the tool "verifycap" cannot be found or called. The error message also sets the path in double quotes. ""/path/to/jc305u1_kit/bin/verifycap""
 The verifycap is available as batch file (original by oracle), as bash shell file with and without *.sh ending

 
#!/bin/bash

# Dieses Script ist eine Linuxportierung.
# Copyright (c) 1998, 2021, Oracle and/or its affiliates. All rights reserved.

# check if JAVA_HOME environment variable is set
if [ "$JAVA_HOME" != "" ]; then
  echo "ERROR : JAVA_HOME not properly defined. Could not find java."
  exit
fi
 
# check if JC_CLASSIC_HOME environment variable is set
if [ "$JC_CLASSIC_HOME" == "" ]; then
  echo "ERROR : Could not find JavaCard Classic in PATH. Please define JC_CLASSIC_HOME."
  exit
fi

# set classpath to all jars
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/ant-contrib-1.0b3.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/api_classic_annotations.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/asm-all-3.1.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/commons-cli-1.0.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/commons-codec-1.3.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/commons-httpclient-3.0.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/commons-logging-1.1.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/jctasks.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/tools.jar:$JC_CLASSPATH"
JC_CLASSPATH="$JC_CLASSIC_HOME/lib/api_classic.jar:$JC_CLASSPATH"

"$JAVA_HOME" "-Djc.home=$JC_CLASSIC_HOME" -classpath "$JC_CLASSPATH" com.sun.javacard.offcardverifier.Verifier "$@"

The path variables are correct and the oracle tools are working fine so far (at least with ant script).

But there are also some additional errors behind the curtain.

Problems occurred when invoking code from plug-in: "org.eclipse.core.resources".

java.lang.StringIndexOutOfBoundsException: begin 0, end -1, length 1
at java.base/java.lang.String.checkBoundsBeginEnd(String.java:3751)
at java.base/java.lang.String.substring(String.java:1907)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.checkJavaVersionCompatibilityForCapFileVerifier(VerifierBuilder.java:406)
at com.nxp.id.jcop.eclipse.internal.builder.VerifierBuilder.build(VerifierBuilder.java:72)
at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:853)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:232)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:281)
at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:334)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:337)
at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:389)
at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:410)
at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:516)
at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:413)
at org.eclipse.ui.actions.BuildAction$1.runInWorkspace(BuildAction.java:291)
at org.eclipse.core.internal.resources.InternalWorkspaceJob.run(InternalWorkspaceJob.java:42)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

The specified file not found or not readable.

java.lang.Exception: The specified file not found or not readable.
at com.nxp.id.jcop.eclipse.core.module.ChecksumGenerator.generateCheckSum(ChecksumGenerator.java:31)
at com.nxp.id.jcop.eclipse.targetpacks.internal.Extension02Simulation.launch(Extension02Simulation.java:537)
at com.nxp.id.jcop.eclipse.internal.launcher.JavaCardLaunchConfigurationDelegate.launch(JavaCardLaunchConfigurationDelegate.java:284)
at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:803)
at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:716)
at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1021)
at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1224)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

Plug-in "com.nxp.id.jcop.eclipse" was unable to instantiate class "com.nxp.id.jcop.eclipse.internal.launcher.JnutTerminalProvider".

java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.base/java.lang.reflect.Constructor.newInstanceWithCaller(Constructor.java:499)
at java.base/java.lang.reflect.Constructor.newInstance(Constructor.java:480)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:204)
at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:920)
at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:246)
at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:63)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager$ReaderProviderExt.getProvider(ReaderManager.java:183)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.update(ReaderManager.java:149)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.__getReaders(ReaderManager.java:100)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.getReaders(ReaderManager.java:79)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.TargetTab.<init>(TargetTab.java:118)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.JavaCardTabGroup.createTabs(JavaCardTabGroup.java:60)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupWrapper.createTabs(LaunchConfigurationTabGroupWrapper.java:133)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$5(LaunchConfigurationTabGroupViewer.java:982)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.createGroup(LaunchConfigurationTabGroupViewer.java:990)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.showInstanceTabsFor(LaunchConfigurationTabGroupViewer.java:896)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.displayInstanceTabs(LaunchConfigurationTabGroupViewer.java:845)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$4(LaunchConfigurationTabGroupViewer.java:727)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.inputChanged(LaunchConfigurationTabGroupViewer.java:742)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput0(LaunchConfigurationTabGroupViewer.java:674)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput(LaunchConfigurationTabGroupViewer.java:654)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.handleLaunchConfigurationSelectionChanged(LaunchConfigurationsDialog.java:1049)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.lambda$1(LaunchConfigurationsDialog.java:612)
at org.eclipse.jface.viewers.StructuredViewer$3.run(StructuredViewer.java:821)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:174)
at org.eclipse.jface.viewers.StructuredViewer.firePostSelectionChanged(StructuredViewer.java:818)
at org.eclipse.jface.viewers.StructuredViewer.setSelection(StructuredViewer.java:1661)
at org.eclipse.jface.viewers.TreeViewer.setSelection(TreeViewer.java:1082)
at org.eclipse.jface.viewers.Viewer.setSelection(Viewer.java:376)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.doInitialTreeSelection(LaunchConfigurationsDialog.java:658)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.initializeContent(LaunchConfigurationsDialog.java:1185)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.createContents(LaunchConfigurationsDialog.java:473)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.create(LaunchConfigurationsDialog.java:378)
at org.eclipse.jface.window.Window.open(Window.java:788)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.open(LaunchConfigurationsDialog.java:1238)
at org.eclipse.debug.ui.DebugUITools.lambda$1(DebugUITools.java:630)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:636)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:574)
at org.eclipse.debug.ui.actions.OpenLaunchDialogAction.run(OpenLaunchDialogAction.java:85)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:414)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1548)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1531)
at org.eclipse.swt.widgets.Widget.notifyListeners(Widget.java:1310)
at org.eclipse.jface.action.ActionContributionItem.lambda$8(ActionContributionItem.java:1207)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5126)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4576)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1150)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1041)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:567)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
Caused by: java.lang.NullPointerException: Cannot invoke "java.lang.reflect.Field.set(Object, Object)" because "this.field" is null
at com.nxp.id.jcop.eclipse.internal.launcher.JnutTerminalProvider.<init>(JnutTerminalProvider.java:94)
... 85 more

and

org.eclipse.core.runtime.CoreException: Plug-in "com.nxp.id.jcop.eclipse" was unable to instantiate class "com.nxp.id.jcop.eclipse.internal.launcher.JnutTerminalProvider".
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.throwException(RegistryStrategyOSGI.java:212)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:206)
at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:920)
at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:246)
at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:63)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager$ReaderProviderExt.getProvider(ReaderManager.java:183)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.update(ReaderManager.java:149)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.__getReaders(ReaderManager.java:100)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.getReaders(ReaderManager.java:79)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.TargetTab.<init>(TargetTab.java:118)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.JavaCardTabGroup.createTabs(JavaCardTabGroup.java:60)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupWrapper.createTabs(LaunchConfigurationTabGroupWrapper.java:133)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$5(LaunchConfigurationTabGroupViewer.java:982)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.createGroup(LaunchConfigurationTabGroupViewer.java:990)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.showInstanceTabsFor(LaunchConfigurationTabGroupViewer.java:896)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.displayInstanceTabs(LaunchConfigurationTabGroupViewer.java:845)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$4(LaunchConfigurationTabGroupViewer.java:727)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.inputChanged(LaunchConfigurationTabGroupViewer.java:742)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput0(LaunchConfigurationTabGroupViewer.java:674)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput(LaunchConfigurationTabGroupViewer.java:654)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.handleLaunchConfigurationSelectionChanged(LaunchConfigurationsDialog.java:1049)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.lambda$1(LaunchConfigurationsDialog.java:612)
at org.eclipse.jface.viewers.StructuredViewer$3.run(StructuredViewer.java:821)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:174)
at org.eclipse.jface.viewers.StructuredViewer.firePostSelectionChanged(StructuredViewer.java:818)
at org.eclipse.jface.viewers.StructuredViewer.setSelection(StructuredViewer.java:1661)
at org.eclipse.jface.viewers.TreeViewer.setSelection(TreeViewer.java:1082)
at org.eclipse.jface.viewers.Viewer.setSelection(Viewer.java:376)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.doInitialTreeSelection(LaunchConfigurationsDialog.java:658)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.initializeContent(LaunchConfigurationsDialog.java:1185)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.createContents(LaunchConfigurationsDialog.java:473)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.create(LaunchConfigurationsDialog.java:378)
at org.eclipse.jface.window.Window.open(Window.java:788)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.open(LaunchConfigurationsDialog.java:1238)
at org.eclipse.debug.ui.DebugUITools.lambda$1(DebugUITools.java:630)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:636)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:574)
at org.eclipse.debug.ui.actions.OpenLaunchDialogAction.run(OpenLaunchDialogAction.java:85)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:414)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1548)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1531)
at org.eclipse.swt.widgets.Widget.notifyListeners(Widget.java:1310)
at org.eclipse.jface.action.ActionContributionItem.lambda$8(ActionContributionItem.java:1207)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5126)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4576)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1150)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1041)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:567)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
Caused by: java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.base/java.lang.reflect.Constructor.newInstanceWithCaller(Constructor.java:499)
at java.base/java.lang.reflect.Constructor.newInstance(Constructor.java:480)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:204)
... 79 more
Caused by: java.lang.NullPointerException: Cannot invoke "java.lang.reflect.Field.set(Object, Object)" because "this.field" is null
at com.nxp.id.jcop.eclipse.internal.launcher.JnutTerminalProvider.<init>(JnutTerminalProvider.java:94)
... 85 more

sys_paths

java.lang.NoSuchFieldException: sys_paths
at java.base/java.lang.Class.getDeclaredField(Class.java:2549)
at com.nxp.id.jcop.eclipse.internal.launcher.JnutTerminalProvider.<init>(JnutTerminalProvider.java:66)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.base/java.lang.reflect.Constructor.newInstanceWithCaller(Constructor.java:499)
at java.base/java.lang.reflect.Constructor.newInstance(Constructor.java:480)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:204)
at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:920)
at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:246)
at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:63)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager$ReaderProviderExt.getProvider(ReaderManager.java:183)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.update(ReaderManager.java:149)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.__getReaders(ReaderManager.java:100)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.getReaders(ReaderManager.java:79)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.TargetTab.<init>(TargetTab.java:118)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.JavaCardTabGroup.createTabs(JavaCardTabGroup.java:60)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupWrapper.createTabs(LaunchConfigurationTabGroupWrapper.java:133)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$5(LaunchConfigurationTabGroupViewer.java:982)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.createGroup(LaunchConfigurationTabGroupViewer.java:990)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.showInstanceTabsFor(LaunchConfigurationTabGroupViewer.java:896)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.displayInstanceTabs(LaunchConfigurationTabGroupViewer.java:845)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$4(LaunchConfigurationTabGroupViewer.java:727)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.inputChanged(LaunchConfigurationTabGroupViewer.java:742)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput0(LaunchConfigurationTabGroupViewer.java:674)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput(LaunchConfigurationTabGroupViewer.java:654)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.handleLaunchConfigurationSelectionChanged(LaunchConfigurationsDialog.java:1049)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.lambda$1(LaunchConfigurationsDialog.java:612)
at org.eclipse.jface.viewers.StructuredViewer$3.run(StructuredViewer.java:821)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:174)
at org.eclipse.jface.viewers.StructuredViewer.firePostSelectionChanged(StructuredViewer.java:818)
at org.eclipse.jface.viewers.StructuredViewer.setSelection(StructuredViewer.java:1661)
at org.eclipse.jface.viewers.TreeViewer.setSelection(TreeViewer.java:1082)
at org.eclipse.jface.viewers.Viewer.setSelection(Viewer.java:376)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.doInitialTreeSelection(LaunchConfigurationsDialog.java:658)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.initializeContent(LaunchConfigurationsDialog.java:1185)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.createContents(LaunchConfigurationsDialog.java:473)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.create(LaunchConfigurationsDialog.java:378)
at org.eclipse.jface.window.Window.open(Window.java:788)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.open(LaunchConfigurationsDialog.java:1238)
at org.eclipse.debug.ui.DebugUITools.lambda$1(DebugUITools.java:630)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:636)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:574)
at org.eclipse.debug.ui.actions.OpenLaunchDialogAction.run(OpenLaunchDialogAction.java:85)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:414)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1548)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1531)
at org.eclipse.swt.widgets.Widget.notifyListeners(Widget.java:1310)
at org.eclipse.jface.action.ActionContributionItem.lambda$8(ActionContributionItem.java:1207)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5126)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4576)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1150)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1041)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:567)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)

Plug-in "com.nxp.id.jcop.eclipse" was unable to instantiate class "com.nxp.id.jcop.eclipse.internal.launcher.SCCommProvider".

org.eclipse.core.runtime.CoreException: Plug-in "com.nxp.id.jcop.eclipse" was unable to instantiate class "com.nxp.id.jcop.eclipse.internal.launcher.SCCommProvider".
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.throwException(RegistryStrategyOSGI.java:212)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:206)
at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:920)
at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:246)
at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:63)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager$ReaderProviderExt.getProvider(ReaderManager.java:183)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.update(ReaderManager.java:149)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.__getReaders(ReaderManager.java:100)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.getReaders(ReaderManager.java:79)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.TargetTab.<init>(TargetTab.java:118)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.JavaCardTabGroup.createTabs(JavaCardTabGroup.java:60)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupWrapper.createTabs(LaunchConfigurationTabGroupWrapper.java:133)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$5(LaunchConfigurationTabGroupViewer.java:982)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.createGroup(LaunchConfigurationTabGroupViewer.java:990)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.showInstanceTabsFor(LaunchConfigurationTabGroupViewer.java:896)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.displayInstanceTabs(LaunchConfigurationTabGroupViewer.java:845)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$4(LaunchConfigurationTabGroupViewer.java:727)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.inputChanged(LaunchConfigurationTabGroupViewer.java:742)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput0(LaunchConfigurationTabGroupViewer.java:674)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput(LaunchConfigurationTabGroupViewer.java:654)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.handleLaunchConfigurationSelectionChanged(LaunchConfigurationsDialog.java:1049)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.lambda$1(LaunchConfigurationsDialog.java:612)
at org.eclipse.jface.viewers.StructuredViewer$3.run(StructuredViewer.java:821)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:174)
at org.eclipse.jface.viewers.StructuredViewer.firePostSelectionChanged(StructuredViewer.java:818)
at org.eclipse.jface.viewers.StructuredViewer.setSelection(StructuredViewer.java:1661)
at org.eclipse.jface.viewers.TreeViewer.setSelection(TreeViewer.java:1082)
at org.eclipse.jface.viewers.Viewer.setSelection(Viewer.java:376)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.doInitialTreeSelection(LaunchConfigurationsDialog.java:658)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.initializeContent(LaunchConfigurationsDialog.java:1185)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.createContents(LaunchConfigurationsDialog.java:473)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.create(LaunchConfigurationsDialog.java:378)
at org.eclipse.jface.window.Window.open(Window.java:788)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.open(LaunchConfigurationsDialog.java:1238)
at org.eclipse.debug.ui.DebugUITools.lambda$1(DebugUITools.java:630)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:636)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:574)
at org.eclipse.debug.ui.actions.OpenLaunchDialogAction.run(OpenLaunchDialogAction.java:85)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:414)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1548)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1531)
at org.eclipse.swt.widgets.Widget.notifyListeners(Widget.java:1310)
at org.eclipse.jface.action.ActionContributionItem.lambda$8(ActionContributionItem.java:1207)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5126)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4576)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1150)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1041)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:567)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
Caused by: java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.base/java.lang.reflect.Constructor.newInstanceWithCaller(Constructor.java:499)
at java.base/java.lang.reflect.Constructor.newInstance(Constructor.java:480)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:204)
... 79 more
Caused by: java.lang.NullPointerException: Cannot invoke "java.lang.reflect.Field.set(Object, Object)" because "this.field" is null
at com.nxp.id.jcop.eclipse.internal.launcher.SCCommProvider.<init>(SCCommProvider.java:104)
... 85 more

and

java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.base/java.lang.reflect.Constructor.newInstanceWithCaller(Constructor.java:499)
at java.base/java.lang.reflect.Constructor.newInstance(Constructor.java:480)
at org.eclipse.core.internal.registry.osgi.RegistryStrategyOSGI.createExecutableExtension(RegistryStrategyOSGI.java:204)
at org.eclipse.core.internal.registry.ExtensionRegistry.createExecutableExtension(ExtensionRegistry.java:920)
at org.eclipse.core.internal.registry.ConfigurationElement.createExecutableExtension(ConfigurationElement.java:246)
at org.eclipse.core.internal.registry.ConfigurationElementHandle.createExecutableExtension(ConfigurationElementHandle.java:63)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager$ReaderProviderExt.getProvider(ReaderManager.java:183)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.update(ReaderManager.java:149)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.__getReaders(ReaderManager.java:100)
at com.nxp.id.jcop.eclipse.internal.launcher.ReaderManager.getReaders(ReaderManager.java:79)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.TargetTab.<init>(TargetTab.java:118)
at com.nxp.id.jcop.eclipse.internal.ui.launcher.JavaCardTabGroup.createTabs(JavaCardTabGroup.java:60)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupWrapper.createTabs(LaunchConfigurationTabGroupWrapper.java:133)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$5(LaunchConfigurationTabGroupViewer.java:982)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.createGroup(LaunchConfigurationTabGroupViewer.java:990)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.showInstanceTabsFor(LaunchConfigurationTabGroupViewer.java:896)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.displayInstanceTabs(LaunchConfigurationTabGroupViewer.java:845)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.lambda$4(LaunchConfigurationTabGroupViewer.java:727)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.inputChanged(LaunchConfigurationTabGroupViewer.java:742)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput0(LaunchConfigurationTabGroupViewer.java:674)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationTabGroupViewer.setInput(LaunchConfigurationTabGroupViewer.java:654)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.handleLaunchConfigurationSelectionChanged(LaunchConfigurationsDialog.java:1049)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.lambda$1(LaunchConfigurationsDialog.java:612)
at org.eclipse.jface.viewers.StructuredViewer$3.run(StructuredViewer.java:821)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
at org.eclipse.jface.util.SafeRunnable.run(SafeRunnable.java:174)
at org.eclipse.jface.viewers.StructuredViewer.firePostSelectionChanged(StructuredViewer.java:818)
at org.eclipse.jface.viewers.StructuredViewer.setSelection(StructuredViewer.java:1661)
at org.eclipse.jface.viewers.TreeViewer.setSelection(TreeViewer.java:1082)
at org.eclipse.jface.viewers.Viewer.setSelection(Viewer.java:376)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.doInitialTreeSelection(LaunchConfigurationsDialog.java:658)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.initializeContent(LaunchConfigurationsDialog.java:1185)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.createContents(LaunchConfigurationsDialog.java:473)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.create(LaunchConfigurationsDialog.java:378)
at org.eclipse.jface.window.Window.open(Window.java:788)
at org.eclipse.debug.internal.ui.launchConfigurations.LaunchConfigurationsDialog.open(LaunchConfigurationsDialog.java:1238)
at org.eclipse.debug.ui.DebugUITools.lambda$1(DebugUITools.java:630)
at org.eclipse.swt.custom.BusyIndicator.showWhile(BusyIndicator.java:74)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:636)
at org.eclipse.debug.ui.DebugUITools.openLaunchConfigurationDialogOnGroup(DebugUITools.java:574)
at org.eclipse.debug.ui.actions.OpenLaunchDialogAction.run(OpenLaunchDialogAction.java:85)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:414)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1548)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1531)
at org.eclipse.swt.widgets.Widget.notifyListeners(Widget.java:1310)
at org.eclipse.jface.action.ActionContributionItem.lambda$8(ActionContributionItem.java:1207)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:5884)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1522)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:5126)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:4576)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1150)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1041)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:78)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.base/java.lang.reflect.Method.invoke(Method.java:567)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
Caused by: java.lang.NullPointerException: Cannot invoke "java.lang.reflect.Field.set(Object, Object)" because "this.field" is null
at com.nxp.id.jcop.eclipse.internal.launcher.SCCommProvider.<init>(SCCommProvider.java:104)
... 85 more

Because of the many errors I also already assumed a faulty installation and have reinstalled both eclipse and the plugin, but the error set remains the same.

Also there appears an error in the settings menu. Window → JCOP → External Offcard Verifier

The current displayed page contains invalid values.

The second click on that menu opens the tab, but everything is blank. When I add the additional values manually, the problem is not fixed.

Does anyone have any tips or ideas on what else I can do to solve this problem?

0 Kudos
Reply

5,453 Views
Tobias_Ehrlich
Contributor I

I have asked our admin to reinstall all drivers and see why the plug-in is not working as expected. We found out that under an admin account everything works (with and also without sudo). The samples are compiled and also the run command works fine. With a user account without the possibility to call sudo it does not work. Further research revealed that the cause is eclipse. For some reason eclipse can't access all resources and has no write permissions in some places, even if all folders and files in the eclipse folders and workspace got chmod 777, eclipse still throws the same error, a different installation directory (e.g. under usr) unfortunately doesn't help here either.

However, the debug mode works partially, also the separate/manual execution of the tools works without problems.

0 Kudos
Reply

5,562 Views
Tobias_Ehrlich
Contributor I
After some testing the best result comes with eclipse photon Java EE x86, there are only 2 errors and no warnings. One is the JnutTerminalProvider, which is not the important thing at the moment (I hope) and also not supported with Linux but the second error is still that one which is required:
 
plugin: com.nxp.id.jcop.eclipse
 
Message:
The specified file not found or not readable.
 
Exception Stack Trace:
java.lang.Exception: The specified file not found or not readable.
at com.nxp.id.jcop.eclipse.core.module.ChecksumGenerator.generateCheckSum(ChecksumGenerator.java:31)
at com.nxp.id.jcop.eclipse.targetpacks.internal.Extension02Simulation.launch(Extension02Simulation.java:537)
at com.nxp.id.jcop.eclipse.internal.launcher.JavaCardLaunchConfigurationDelegate.launch(JavaCardLaunchConfigurationDelegate.java:284)
at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:859)
at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:717)
at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1039)
at org.eclipse.debug.internal.ui.DebugUIPlugin$8.run(DebugUIPlugin.java:1256)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:60)
 
Session Data:
eclipse.buildId=4.8.0.I20180611-0500
java.version=1.8.0_291
java.vendor=Oracle Corporation
BootLoader constants: OS=linux, ARCH=x86, WS=gtk, NL=de_DE
Framework arguments: -product org.eclipse.epp.package.jee.product
Command-line arguments: -os linux -ws gtk -arch x86 -product org.eclipse.epp.package.jee.product
 
Also I did some reverse engineering and I couldn't find some build packages:
  • com.nxp.id.jcop.eclipse.jcopbuilder
  • com.nxp.id.jcop.eclipse.jcopbuildverifier

Where are they hidden?

0 Kudos
Reply

6,201 Views
msjcard
Contributor III

Finally got this to work with most recent version of tools AND only Eclipse Kepler Java EE.