Is it possible to use the OM-SE050ARD kit together with non-NXP boards?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use the OM-SE050ARD kit together with non-NXP boards?

1,860件の閲覧回数
jordijofrenxp
NXP Employee
NXP Employee

Yes, it is. On the one hand, if you are using an Arduino-compatible MCU board, you can connect it using the Arduino connectors. On the other hand, if you are using a non-Arduino board, you can connect it using the external I2C connector

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)