In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

1,637 次查看
jordijofrenxp
NXP Employee
NXP Employee

The ISO/IEC 14443 interface of the EdgeLock SE050 gives you the capability to communicate with any NFC phone or contactless reader. Key applications include systems that require late stage product customization, including zero-power configuration and trust provisioning over a contactless reader.

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数