Dear NXP support team,
I would like to use ISO7816 interface in SE050.
(i) Can the following environment use ISO7816 interface?
- EdgeLock® SE050 Development Kit
- SE050C2 chip
(ii) If answer of (i) is "yes", would you tell me what document should I refer to in order to use ISO7816 interface?
Best Regards,
Masahiro Marume
已解决! 转到解答。
Hi @masa_m ,
Actually this kind of interface is just available with some custom type of SE050. You have to contact your local NXP Marketing/sales or local FAE for further help.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @masa_m ,
I am sorry, but this kind of interface is not supported in the following environment:
- EdgeLock® SE050 Development Kit
- SE050C2 chip
Only the following interfaces are available.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kan,
Thank you for your response.
Would you tell me which environment supports ISO7816 interface?
I found the following description in SE050 datasheet
So, I thought SE050 can use ISO7816 interface.
Regards,
Masahiro Marume
Hi @masa_m ,
Actually this kind of interface is just available with some custom type of SE050. You have to contact your local NXP Marketing/sales or local FAE for further help.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------