Hi @krsuresh ,
SE05x supports writing private key into this device if the policy of the key object allows, but not possible to read the private key out of the device.
The bin file length can reach up to 0x7FFF but also limited by the free space left in the device when you create this bin file.
The APDU commands can be used to create/write or read the secure objects in the device, but for application purpose, I would recommend the SSS APIs out of the Plug&Trust MW. You may refer to the demo of ex_ecc or ex_rsa for more details.
Please kindly refer to https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-and-trus... for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------