Page 8 of AN12395 indicates that J14 must be set to postion 1-2 to enable deep power-down mode. I believe this is incorrect. According to the description given, Figure 6, and the settings shown in Table 4, I think it should read:
I don't have one of these boards to validate this. I am just reading through documentation getting ready to build a prototype with the SE050.
Hello @jaredl ,
Actually in earlier version it is 3-4 for J14 indeed, but I am not sure if it is due to hardware version difference, let me check it with the expert .
Thanks for the report!
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------