Do not use ISO7816/14443 interface in SE050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do not use ISO7816/14443 interface in SE050

跳至解决方案
2,653 次查看
george
Senior Contributor II

Dear NXP team,

We will use SE050 for our new product.

However, our product does not use ISO7816 and ISO14443 Interfaces.

pastedImage_1.png

ISO_14443_LA

ISO_14443_LB

ISO_7816_RST

ISO_7816_CLK

ISO_7816_IO

ISO_7816_IO2

How should these pins be terminated?

Best Regards,

George

1 解答
2,442 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
2,443 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,442 次查看
george
Senior Contributor II

Dear Kan_Li,

Thank you for your quick reply.

Is my understanding correct below?

pastedImage_1.png

And is the Pull Up/Down value about 10k-ohm appropriate?

BR,

George

0 项奖励
回复
2,442 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi George,

Yes, that is ok.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,442 次查看
george
Senior Contributor II

Thanks,

George

0 项奖励
回复