Do not use ISO7816/14443 interface in SE050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do not use ISO7816/14443 interface in SE050

Jump to solution
2,587 Views
george
Senior Contributor II

Dear NXP team,

We will use SE050 for our new product.

However, our product does not use ISO7816 and ISO14443 Interfaces.

pastedImage_1.png

ISO_14443_LA

ISO_14443_LB

ISO_7816_RST

ISO_7816_CLK

ISO_7816_IO

ISO_7816_IO2

How should these pins be terminated?

Best Regards,

George

1 Solution
2,376 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

4 Replies
2,377 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,376 Views
george
Senior Contributor II

Dear Kan_Li,

Thank you for your quick reply.

Is my understanding correct below?

pastedImage_1.png

And is the Pull Up/Down value about 10k-ohm appropriate?

BR,

George

0 Kudos
Reply
2,376 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi George,

Yes, that is ok.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,376 Views
george
Senior Contributor II

Thanks,

George

0 Kudos
Reply