Do not use ISO7816/14443 interface in SE050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do not use ISO7816/14443 interface in SE050

ソリューションへジャンプ
2,224件の閲覧回数
george
Senior Contributor II

Dear NXP team,

We will use SE050 for our new product.

However, our product does not use ISO7816 and ISO14443 Interfaces.

pastedImage_1.png

ISO_14443_LA

ISO_14443_LB

ISO_7816_RST

ISO_7816_CLK

ISO_7816_IO

ISO_7816_IO2

How should these pins be terminated?

Best Regards,

George

1 解決策
2,013件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,014件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello George,

If not used, ISO7816 interface tied to VCC and ISO14443 interface tie to GND.

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,013件の閲覧回数
george
Senior Contributor II

Dear Kan_Li,

Thank you for your quick reply.

Is my understanding correct below?

pastedImage_1.png

And is the Pull Up/Down value about 10k-ohm appropriate?

BR,

George

0 件の賞賛
返信
2,013件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi George,

Yes, that is ok.

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,013件の閲覧回数
george
Senior Contributor II

Thanks,

George

0 件の賞賛
返信