Denied to read object bases on policy.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Denied to read object bases on policy.

680件の閲覧回数
WorkerEmbedded
Contributor II

Hello to everyone, i've got a problem!

Anyone can tell me why i can't access to an object where previosly i stored a key successfully with the sss_key_store_set_key function.

Now with the sss_key_store_get_key i recive the following sentences:

sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:7026 Function:sss_se05x_TXn
hostLib:WARN :Denied to read object EF000033 bases on policy.
sss :WARN :nxEnsure:'status == SM_OK' failed. At Line:4009 Function:sss_se05x_key_store_get_key

0 件の賞賛
返信
1 返信

666件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @WorkerEmbedded ,

 

Maybe due to the secure obj's policy, or you have to authenticate to access this obj. BTW, is it possible to delete this obj with the demo of "Delete and Test Provision"?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信