AESKey Session Authentication for SE050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AESKey Session Authentication for SE050

2,093 次查看
nana11
Contributor I

Hello,

I'm trying to establish an AESKey secure session with a SE050 board using the Java SmartCard I/O API but am running into authentication issues.

When I send the SCPExternalAuthenticate command, I consistently get a 6700 ("Wrong length") error regardless of what I try.

what works:
1. I can successfully select the SE050 applet
2. I can successfully create an AES key authentication object
3. I can successfully start a session using the created authentication object
4. The SCPInitializeUpdate command completes successfully

log:

Found terminal: Identiv uTrust 3700 F CL Reader
Card is present in Identiv uTrust 3700 F CL Reader
Successfully connected to SE050.
Selecting applet with command: 00A4040010A0000003965453000000010300000000
Select response: SW=9000, Data=0301016FFF010B
SE050 applet selected successfully.
Enter 4-byte object ID for your AES key (8 hex characters, e.g., 12345678):
88888881
Enter 16-byte AES key (32 hex characters):
404142434445464748494A4B4C4D4E4F
Creating session...
CreateSession command: 8004001B064104888888810C
CreateSession response: SW=9000, Data=4182000801A1883AD1C0DDE6
Session created. Session ID: 01A1883AD1C0DDE6
Host challenge: 0F935F37FFC7DD2C
SCPInitializeUpdate command: 8005000019100801A1883AD1C0DDE6410D80500000080F935F37FFC7DD2C
SCPInitializeUpdate response: SW=9000, Data=000000000000000000000003606897205702C2B9EF8AC6E05E6B26EB83
Key diversification data: 00000000000000000000
Key info: 00
Card challenge: 03606897205702C2
Card cryptogram: B9EF8AC6E05E6B26
Derived S-ENC key: E2D59DD0015AA32B377A5CC6EED41DE6
Derived S-MAC key: 3458D77ADD4D1BF923D10367959E4C4B
Derived S-RMAC key: BC7323AE62CF71AD7DC3C59D56D1AFA6
Expected card cryptogram: 88612A8EC56FA45C
Card cryptogram doesn't match expected value, but proceeding anyway...
Host cryptogram: 88612A8EC56FA45C
SCPExternalAuthenticate command: 8005000021100801A1883AD1C0DDE64115848203000888612A8EC56FA45C5AD68E843A534B64
SCPExternalAuthenticate response: SW=6700, Data=
Authentication failed.

my SE050 details:
Applet Select Response Information:
Major: 3
Minor: 1
Patch: 1
AppletConfig: 0x6fff
SE050 Variant: SE050E2 (FIPS mode enabled)
Secure Box version: 1.b

what i need to check when i SCPExternalAuthenticate? 

thanks

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

2,071 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nana11 ,

 

Was your SE050 provisioned for demo purpose? Please kindly refer to se05x_mw_v04.05.01/simw-top/doc/demos/se05x/se05x_Delete_and_test_provision/Readme.html for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复