AES-GCM performance on SE05x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AES-GCM performance on SE05x

317 次查看
Viktro0929
Contributor II

I am testing the capabilities of the SE050 on an OM-SE050X development board, and I have a question about the speed of the AES-GCM operation. It seems that when running a one-shot AES-GCM encryption with AAD, followed by decryption, the process takes around 8 to 9 seconds, even with small inputs in one-shot mode

I found a similar thread here discussing the same issue:

https://community.nxp.com/t5/Secure-Authentication/Re-SE050E-aead-encryption/m-p/1694085#M1317

The response there indicated that this is indeed expected, since the GCM part is not hardware-accelerated.

 

My questions are:

  • Can you please confirm whether this speed is normal, and whether there is any way to improve performance, or if software-based GCM will remain at this speed regardless?
  • Regarding the SE051 (or SE052), do these chips provide hardware acceleration for GCM, or any improvements in the speed of this operation?

 

Thank you in advance!

标签 (1)
0 项奖励
回复
5 回复数

298 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Viktro0929 ,

 

Was it AES GCM 128 or 256? What about the data/AAD/IV length? From the test cases we have run, 8 to 9 seconds is little longer, what is the host controller you are using? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

268 次查看
Viktro0929
Contributor II

I am using test vectors from Test Case 3 of the following document:
https://csrc.nist.rip/groups/ST/toolkit/BCM/documents/proposedmodes/gcm/gcm-revised-spec.pdf 

 

Configuration details:

  • AES-GCM 128-bit (16-byte key length)

  • Data length: 60 bytes

  • AAD length: 20 bytes

  • IV length: 12 bytes

 

My OM-SE050X is connected to an ATSAMV71Q21 via I²C running at 100 kHz.

I have attached a screenshot of a typical encryption. As shown, after the initial setup, the host sends the plaintext and AAD, and the SE subsequently requests 5 WTXs. The WTX time was calculated based on the ATR response and the WTX message itself (as described in UM11225.pdf).

In total, the encryption process (including setup) took just under 7 seconds, of which about 1 second was spent in setup.

se050-aesgcm-logicanalyzer.PNG

 

Thank you!

 

Best regards,

Viktor

0 项奖励
回复

251 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Viktro0929 ,

 

Actually our test case is a little bit different from yours, please kindly refer to the following for details.

  • AES-GCM 128-bit (16-byte key length)

  • Data length: 64 bytes

  • AAD length: 16 bytes

  • IV length: 16 bytes

Both encrypt and decrypt took around 5.4 second. You may try the same on your side .

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复

246 次查看
Viktro0929
Contributor II

Thank you, I will try this out when I have some free time.

Beforehand, could you please clarify the second part of my original question? Specifically:

  • Regarding the SE051 (or SE052), do these chips provide hardware acceleration for GCM, or any improvements in the speed of this operation compared to the SE050?
  • If yes, how much faster is the performance compared to SE050 for similar message sizes, such as your test case?
0 项奖励
回复

101 次查看
Viktro0929
Contributor II

Hi @Kan_Li ,

Just following up on my earlier message about the SE051/SE052. Could you please clarify whether these devices have any hardware acceleration for GCM, or performance improvements over the SE050? If so, by how much?

Thank you!

0 项奖励
回复