Hi,
I am working on the development board of A71CH [A71CH | Plug and Trust for IoT|NXP ]
I am following the document AN12135 [https://www.nxp.com/docs/en/application-note/AN12135.pdf ] to integrate A71CH with Kinetics board [FRDM k64F].
In the documentation, I am supposed to download a software package The A71CH Host software package called [A71CH_HOST_SW].
link: Version 01.04.00 (or later), available on [A71CH | Plug and Trust for IoT|NXP - A71CH Host Software Package (Windows Installer)]
But this software package does not provide me the required examples to run the demos mentioned in AN2135.
I do not have required examples of vcomA71CH. I have added the screenshots of pages from documentation which is missing when I download the required software packages. In below attachments, I cannot find what is mentioned in Capture 1 image.
Can someone send the package with this reply?
It would be great if I could get this help. My research work is based on this. I am not able to proceed.
Thanks and Regards,
Niranjan.
3177289354.
已解决! 转到解答。
Hi,
Did you download the latest version(A71CH_v1.4.3.0)? The projects are right there, please refer to the following for details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Did you download the latest version(A71CH_v1.4.3.0)? The projects are right there, please refer to the following for details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------