Hi,
Can you confirm if the FCCU monitoring functionality is available on the VR5510 ASIL B chipset? It seems to be unclear to me from the VR5510 Safety Manual. Table 5 indicates that is is available but Table 9 indicates it is not available.
解決済! 解決策の投稿を見る。
Yes I have confirmed the Safety manual will need to be fixed
The Watchdog difference is noteable
FCCU is available for ASIL-B version
From section 22 in the datasheet
Thanks Daniel but in the VR5510 Safety Manual User Guide on page 26 Table 9. 'Fail-safe OTP configuration' it show that the register entry to enable the FCCU monitoring is only available in ASIL D chips. Can you confirm that this is the case? If so then the table you are referring to is inaccurate?
Many thanks,
Nick
Hi Daniel,
So to confirm your saying the VR5510 Safety Manual document is incorrect and the FCCU monitoring is in fact available on the ASILB chipset?
Yes I have confirmed the Safety manual will need to be fixed
The Watchdog difference is noteable