SAR_ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,255 Views
HeebeomPark
Contributor II

 

 

• SM4.REDUNDANT_IO is for ASIL D 99% DC?

For us, we required the DC corresponding to ASIL B. 

In this case, which safety mechanism can be alternative instead of SM.REDUNDANT_IO?

HeebeomPark_0-1699269094569.png

 

0 Kudos
1 Solution
1,180 Views
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

View solution in original post

0 Kudos
3 Replies
1,189 Views
HeebeomPark
Contributor II

Thank you very much for your answer.

What do you mean "have to stop the application and run this test"? Can you specify in term of the implementation perspective? 

0 Kudos
1,181 Views
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

0 Kudos
1,197 Views
ehtesham_khan
NXP Employee
NXP Employee

Hello,

The ADC Self-test (SM1.ADC_SELF_TEST)- Periodic test of correct ADC operation, can be done in place of SM4.REDUNDANT_IO for ASIL-B application. 

The ADC Self-test will not be able to run with the application, you'll have to stop the application and run this test, then resume the application. Run this test periodically, once per FHTI, to get sufficient coverage.

 

Regards,
Ehtesham

 

0 Kudos