SAR_ADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,491 次查看
HeebeomPark
Contributor II

 

 

• SM4.REDUNDANT_IO is for ASIL D 99% DC?

For us, we required the DC corresponding to ASIL B. 

In this case, which safety mechanism can be alternative instead of SM.REDUNDANT_IO?

HeebeomPark_0-1699269094569.png

 

0 项奖励
1 解答
1,416 次查看
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

在原帖中查看解决方案

0 项奖励
3 回复数
1,425 次查看
HeebeomPark
Contributor II

Thank you very much for your answer.

What do you mean "have to stop the application and run this test"? Can you specify in term of the implementation perspective? 

0 项奖励
1,417 次查看
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

0 项奖励
1,433 次查看
ehtesham_khan
NXP Employee
NXP Employee

Hello,

The ADC Self-test (SM1.ADC_SELF_TEST)- Periodic test of correct ADC operation, can be done in place of SM4.REDUNDANT_IO for ASIL-B application. 

The ADC Self-test will not be able to run with the application, you'll have to stop the application and run this test, then resume the application. Run this test periodically, once per FHTI, to get sufficient coverage.

 

Regards,
Ehtesham

 

0 项奖励