SAF or SPD for S32K3 with ASIL B allocated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAF or SPD for S32K3 with ASIL B allocated

1,020 Views
zeyu_yan
Contributor III

Hi 

     I want to know, is it enough to use SPD(Safety Peripheral Drivers) for S32K3 while it is allocated with ASIL B? 

      or must we use safety software framework instead which is not free?

zeyu_yan_0-1665640340223.png

 

Labels (1)
Tags (3)
1 Reply

1,006 Views
aarul
NXP Employee
NXP Employee

Hi

The use of SAF is not mandatory to achieve the required safety integrity. However, it is important to fulfill the assumptions in the Safety Manual and SAF/SCST are NXP software offerings then enable customers to implement these assumptions easily. If you are not using these SW components, then you may have to develop your own Software to fulfill the assumptions.

Regards

-Aarul

0 Kudos