S32K324's FMEDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K324's FMEDA

1,089 Views
WeoWang
NXP Employee
NXP Employee

Hi Dear Colleagues, 

I notice that there is only ASIL-D S32K324's FMEDA in the community, do we have an ASIL-B version? Or if the customer only needs ASIL-B, can they just use the ASIL-D version? Thanks.

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,079 Views
ehtesham_khan
NXP Employee
NXP Employee

Hello Weo Wang,

The S32K324 is for the ASIL-B use-case only. The FMEDA on the community is for ASIL-B https://community.nxp.com/t5/SafeAssure-NDA-group/FMEDA-SEooC-Static-S32K324/ta-p/1218274
If customer wants to use in the ASIL-D use-case, they need to use S32K344.

0 Kudos

1,078 Views
aarul
NXP Employee
NXP Employee

Hello Weo Wang

Just to add to Ehtesham's response,

Note that the FMEDAs are based on the NXP's assumed safety concept where we target split-lock cores (S32K324) for ASIL-B application and lockstep for ASIL-D application (S32K344). These FMEDAs are based on specific configuration and NXP provides some flexibility to re-configure the FMEDA for customer's usecase.

You should review the safety manual/concept and evaluate if you require to customize the FMEDA or the existing FMEDAs are sufficient for you.

 

Regards

-Aarul

 

0 Kudos