Hi NXP,
I'm working with MCU S32K146, I want to understand the MCU over voltage effect of S32K146. Please help to clarify the following questions:
1. From datasheet, if the Vdd supply voltage is between [5.5V, 5.8V], MCU can operate with no restrictions for 60s lifetime, does this mean within 60s lifetime, the safety mechanism of MCU can still work?
2. Above 5.8V but before MCU damage, MCU software can't operate properly which is the critical failure mode for my application. MCU damage is system safe state for my application. Therefore, could NPX provide the over-voltage threshold which will definitely damage the MCU within 300ms (FTTI of my application), then I can evaluate the dangerous over-voltage range for my application.
Thanks for your support.
Hello,
Here are the answers to your questions:
We must recommend to the customer operates the MCU within the normal operation levels indicated in the DS. See Table 3 in the Datasheet
Best regards,
Oscar Hinojosa.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------