FMEDA - Sheet S32G2 for customer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMEDA - Sheet S32G2 for customer

153 Views

Hello Team,

 My customer (TTTech Auto) requires access to Medini file that can be configured at their end.

In the document “sr565603 - S32G Safety Analysis Report (0.3).pdf” provides the info on the mission profile used for FMEDA calculations is following:

 
KrishnaTirumalaraju_FAE_4-1726832050135.pngKrishnaTirumalaraju_FAE_5-1726832058872.png

 

Unfortunately, the document S32G_FMEDA_ASILB_CONFIG.xls, is not automatic where we can modify the mission profile.

The following changes in the mission profile are requested from customer and would like to generate an updated FMEDA Excel file

1) Temp distribution:

 
KrishnaTirumalaraju_FAE_6-1726832231996.png
2) 
KrishnaTirumalaraju_FAE_7-1726832240869.png

3) If needed, we normally assume 5 cycles per day - so in a year 300*5=1500 on cycles and 65*5=325 off cycles

Could you please provide the access to modify and generate FMEDA from  the customer end. 

 

Thank you, 

Krishna (NXP FAE for TTTech)

 

S32G2 FUNCTIONAL-SAFETY-SYSTEM-BASIS 

Labels (1)
0 Kudos
1 Reply

56 Views
antoinedubois
NXP Employee
NXP Employee

Hi Krishna,

We now share the Medini files with customer from our secure files for S32G. You and customer should be able to download and configure the Mission profile.

the following PPT (currently internal but soon to be relase for Public) explained what can be configured.

If you have any problem finding the file son secure files please contact Bas Wielens.

0 Kudos