EIM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM

446件の閲覧回数
HeebeomPark
Contributor II

Once the safety manual is updated to 6.0, there are some comments for configuration as below in the red box.

Is it only information or what should the user do for this?

HeebeomPark_0-1739182352161.png

 

HeebeomPark_1-1739182370696.png

 

 

0 件の賞賛
3 返答(返信)

284件の閲覧回数
antoinedubois
NXP Employee
NXP Employee

Hi Heebeom, SM2 usually inject failure using the EIM interfaces (not always). If you use NXP SAF Scheck (recommended), you do not need to implement anything else, EIM fault injectino is transparent to you.

0 件の賞賛

361件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

The user needs to do the error injection to be sure that the ECC check is working.

Regards,

John

0 件の賞賛

342件の閲覧回数
HeebeomPark
Contributor II

Normally, SM2(es) are supported to check the functionalities of checkers.

In terms of the purposes, instead of using the SM2 can be sufficient at least for ECC and Gasket and so on?

0 件の賞賛