Debug mode disable in MPC5746C SM: SM_047

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug mode disable in MPC5746C SM: SM_047

Jump to solution
900 Views
BoxLi
NXP Employee
NXP Employee

Hi

I saw there is a statement in MPC5746C Safety Manual Rev2: SM_047''Assumption:[SM_047] Debugging will be disabled in the field while the device is being used for safety-relevant functions. [end]"

My question is how to implement this. There is no detail description here.

I saw in MPC5746R or MPC5744P SM, JCOMP should be pulled high and monitored by FCCU. 

Can you help check and clarify this issue? Thanks.

Labels (1)
Tags (1)
0 Kudos
1 Solution
874 Views
aarul
NXP Employee
NXP Employee

Hi Box Li

This is correct. For fulfilling this assumption:

JCOMP should be pulled low and monitored by FCCU

Regards

-Aarul

PS: Correction Made on pull on JCOMP. JCOMP should be pulled to the value that ensures that the TAP controller is in reset state in field.

View solution in original post

0 Kudos
1 Reply
875 Views
aarul
NXP Employee
NXP Employee

Hi Box Li

This is correct. For fulfilling this assumption:

JCOMP should be pulled low and monitored by FCCU

Regards

-Aarul

PS: Correction Made on pull on JCOMP. JCOMP should be pulled to the value that ensures that the TAP controller is in reset state in field.

0 Kudos