TJA115x FMEDA Information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA115x FMEDA Information

Jump to solution
6,307 Views
biten
Contributor III

Hi,

 

Is it possible to get FMEDA information for the TJA115x CAN PHY?

 

Thanks

0 Kudos
1 Solution
6,276 Views
r40959
NXP Employee
NXP Employee

Hi, 

please find attached information on guidance about the failure modes split and failure rate of TJA115x.

 

we would like to remind

*Disclaimer: The TJA115x device is not ISO26262 developed nor compliant to ISO26262. It is a Quality Managed device AECQ100.
The information on the two slides are for information only and NXP is not responsible on the way the data are used.

best regards

View solution in original post

0 Kudos
7 Replies
6,284 Views
r40959
NXP Employee
NXP Employee

Hello,

the TJA115x is a Quality Managed product (not ISO26262), meaning that we don't have a FMEDA for this CAN transciever.

in order to support, we can provide a list of Functional failure modes corresponding to this product as well as a failure rate input evaluation.

Let us know,

thank you

best regards

Valerie

0 Kudos
6,281 Views
biten
Contributor III

if you could provide that information that would be great. 

Thanks,

Ben

0 Kudos
6,277 Views
r40959
NXP Employee
NXP Employee

Hi, 

please find attached information on guidance about the failure modes split and failure rate of TJA115x.

 

we would like to remind

*Disclaimer: The TJA115x device is not ISO26262 developed nor compliant to ISO26262. It is a Quality Managed device AECQ100.
The information on the two slides are for information only and NXP is not responsible on the way the data are used.

best regards

0 Kudos
6,271 Views
biten
Contributor III

Do you happen to have results for the TJA1153 too? The package is different between the 1152 and 1153.

Thanks for the information already shared this is great. 

0 Kudos
6,268 Views
r40959
NXP Employee
NXP Employee

Hello,

yes, i attach the pdf including TJA1153.

best regards

Valerie

0 Kudos
6,295 Views
naveenm
NXP Employee
NXP Employee

Hi Ben,

I have enquired about your query with concerned person. Unfortunately, she is on leave this week. 

I will update you on 19th July. Hope it works for you.

 

Please let me know if there is anything urgent, I will give it a try with others.

 

Regards,

NaveenM

0 Kudos
6,291 Views
biten
Contributor III

We will plan on waiting until 7/19. Thanks for the update. 

0 Kudos