SM4.FLASH.PGM_ERS_CONTENT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SM4.FLASH.PGM_ERS_CONTENT

1,078 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Customer would like information related to sm815340-S32K3xx Series Safety Manual(4.0) the safety mechanism SM4.FLASH.PGM_ERS_CONTENT

"Is there any document or information which has more details regarding the implementation of this SM.and also should we use DMA for implementing this SM."

0 Kudos
1 Reply

1,058 Views
chokor
NXP Employee
NXP Employee

Hi,

SM4.FLASH.PGM_ERS_CONTENT is an application dependent safety mechanism, here is what to perform (quoted from SM):

"The application software needs to check the contents
of the flash memory after performing flash-memory
programming operations to detect faults in the flash.
This test should be performed after every program
operation or after a series of program operations to
the flash memory.
For doing this, the result of programmed/erased
operation can be based on a read-back scheme, where
the written word is read back and compared with the
intended value.
Alternatively, the safety relevant data can be saved with
a CRC to validate them. The built-in hardware CRC
module can be used for this purpose. [810135]".

Implementation or whether a DMA to be used are customer decisions

0 Kudos