SAR_ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,873件の閲覧回数
HeebeomPark
Contributor II

 

 

• SM4.REDUNDANT_IO is for ASIL D 99% DC?

For us, we required the DC corresponding to ASIL B. 

In this case, which safety mechanism can be alternative instead of SM.REDUNDANT_IO?

HeebeomPark_0-1699269094569.png

 

0 件の賞賛
1 解決策
1,798件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,807件の閲覧回数
HeebeomPark
Contributor II

Thank you very much for your answer.

What do you mean "have to stop the application and run this test"? Can you specify in term of the implementation perspective? 

0 件の賞賛
1,799件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

When running an ADC selftest the ADC will not be able to be used by the application code.  That is what was meant by "have to stop the application and run this test".  Other parts of the application can run that are not using the ADC.

Regards,

John

0 件の賞賛
1,815件の閲覧回数
ehtesham_khan
NXP Employee
NXP Employee

Hello,

The ADC Self-test (SM1.ADC_SELF_TEST)- Periodic test of correct ADC operation, can be done in place of SM4.REDUNDANT_IO for ASIL-B application. 

The ADC Self-test will not be able to run with the application, you'll have to stop the application and run this test, then resume the application. Run this test periodically, once per FHTI, to get sufficient coverage.

 

Regards,
Ehtesham

 

0 件の賞賛