S32K311 PMC VDD_HV_A and VDD_HV_FLA Error Injection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K311 PMC VDD_HV_A and VDD_HV_FLA Error Injection

660 Views
raj12
Contributor III

Hello Team Nxp,

I want to Inject PMC VDD_HV_A and VDD_HV_FLA error and my expectation is FCCU4 should be trigger.

I have query on below mentioned points: - 

1. Go/No-go Indicator for VDD1PD1.
  Specifies whether the VDD1PD1 (double bond) supply going to PLL is clean.
  Read this field to identify the reason for a fault in case of FCCU NCF 4.
  If this field = 1, the "go" indication specifies a clean supply, and if this field = 0, the "no-go"   indication specifies an unclean supply with a fault in the double-bond connection or its routing within the chip. 

2. Go/No-go Indicator For VDD_HV_FLA.
   Specifies whether the VDD_HV_FLA (double bond) supply going to XOSC and PLL is clean.
   Read this field to identify the reason for a fault in case of FCCU NCF 4.
   If this field = 1, the "go" indication specifies a clean supply, and if this field = 0, the "no-go" i        indication specifies an unclean supply with a fault in the double-bond connection or its     routing within the chip. 

3. what is clean voltage supply?

How to perform above scenario for injection of error? 

looking forward for your reply.

Thanks in advance.

0 Kudos
1 Reply

609 Views
antoinedubois
NXP Employee
NXP Employee

This community is no longer supporting. Could you repost your question into the S32K3 Community.

Thank you

0 Kudos