S32K3 Safety Manual Addendum ID 1248005

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 Safety Manual Addendum ID 1248005

跳至解决方案
1,663 次查看
john_floros
NXP Employee
NXP Employee

Hello,

In the Safety Manual Addendum there is an assumption with ID 1248005 that the TEST input is tied to ground during boot and normal operation mode.

The question is what Test input or Test pin is this referring to?

Thank you,

John H. Floros

0 项奖励
1 解答
1,615 次查看
nxf55526
NXP Employee
NXP Employee

Hello John,

This assumption ID 1248005 has been removed from the updated list of assumptions since the S32K3 doesn't include a Test input pin. This would get reflected in the next draft of the Safety Manual. Hope this clarifies. 

Thanks and Regards,

Avni

在原帖中查看解决方案

0 项奖励
1 回复
1,616 次查看
nxf55526
NXP Employee
NXP Employee

Hello John,

This assumption ID 1248005 has been removed from the updated list of assumptions since the S32K3 doesn't include a Test input pin. This would get reflected in the next draft of the Safety Manual. Hope this clarifies. 

Thanks and Regards,

Avni

0 项奖励