S32K1xx - ECC check within FFTI (EIM)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K1xx - ECC check within FFTI (EIM)

1,583 次查看
luca_toso
Contributor II

Hi All,

I already checked this post  and similar other bt I don't find a satisfying answer:

luca_toso_0-1624546718976.png

 

Does this mean that

- the software shall trigger an ECC event on SRAM once per FFTI using the EIM? or

-  the ECC (hence the register relevant for SRAM and FLASH errors) shall be checked once per FTTI?

I assume this is relevant only for double bit errors since they are not correctable. 

Thanks and B.R.

 

L.T. 

 

 

标记 (4)
0 项奖励
5 回复数

1,556 次查看
ehtesham_khan
NXP Employee
NXP Employee

This is a recommendation for additional safety integrity on ECC Logic but not a requirement. If you think that this will impact your system performance it is OK to test it once at startup.

0 项奖励

1,531 次查看
Susan_1
Contributor I
  • What is the impact of testing once at startup on PMHF,SPF,LF.

0 项奖励

1,520 次查看
Yashwant_Singh
NXP Employee
NXP Employee

ECC has very little (almost negligible) contribution to single point fault and is considered primarily as a source of latent faults. So if you are running a check once every MPFDTI, then there should not be any noticeable change in SPF/LFM/PMHF. 

0 项奖励

1,564 次查看
ehtesham_khan
NXP Employee
NXP Employee

This means the software shall trigger an event using EIM to check the ECC in SRAM and Flash and it should check the relevant register once per FTTI. The EIM can inject single bit as well as multi bit errors.

0 项奖励

1,575 次查看
luca_toso
Contributor II

Up, because the topic is relevant for us. 

Triggering an ECC error via EIM once per FFTI is pretty invasive, in our opinion. 

Furthermore, due to the cortex m0 archtiecture the ECC on SRAM in the S32K1xx is first routed to the HardFault Handler and only then to the SRAM error ecc handler, and this is bothersome. If possible, avoiding it would be a pleasure. 

0 项奖励