S32G SAF configuration in S32CT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G SAF configuration in S32CT

2,334 Views
shuangjunzhu
NXP Employee
NXP Employee
 
0 Kudos
5 Replies

2,325 Views
shuangjunzhu
NXP Employee
NXP Employee

Finally, I installed the S32G2 SAF RTM 1.0.1.

But there is no "S32 SAF example project" in the S32 studio. Any comments?

 

Thanks,

Jeff

0 Kudos

2,328 Views
shuangjunzhu
NXP Employee
NXP Employee

But the installation failed:

Software being installed: SAF S32G2XX 1.0.1.202107010823 (com.nxp.SAF.S32G2XX.root.1.0.1.feature.feature.group 1.0.1.202107010823)
  Missing requirement: SAF S32G2XX 1.0.1.202107010823 (com.nxp.SAF.S32G2XX.root.1.0.1.feature.feature.group 1.0.1.202107010823) requires 'org.eclipse.equinox.p2.iu; com.nxp.RTD.S32CC.root.2.0.0.feature 0.0.0' but it could not be found
 

 

 

0 Kudos

2,322 Views
martinkaspar-r3
NXP Employee
NXP Employee

The SAF provides two installers – one installer file for standalone use (S32G_SAF_1.0.1_D2106.exe) and one installer file for use in S32 Design Studio (this one is called update site zip file: S32G_SAF_1.0.1_DS_updatesite.zip). Both installers are available from nxp.com from the same place (after logging with your account). Note that you need to have a valid license to be able to download SAF (NXP internal people can get license for NXP internal use from https://are.nxp.com/FlexNetCatalog.aspx).

The SAF requires RTD 2.0.0 HF2 to be installed in S32 Design Studio. So install first the SW32G2_RTD_4.4_2.0.0_HF02_DS_updatesite_D2106.zip. All the details about SAF installation into S32 Design Studio are described in SAF release notes:

=====

For S32 Design Studio users:

Install the latest version of S32 Design Studio for S32 platform (currently v.3.4).

Prior to installation of the SAF Update Site, please install S32G2 development package

for the Design Studio - SW32G2_S32DS_3.4.0_D2012.zip and RTD Update Site - SW32G2_RTD_4.4_2.0.0_HF02_DS_updatesite_D2106.zip

=====

0 Kudos

2,328 Views
shuangjunzhu
NXP Employee
NXP Employee

I got it in package "S32G2 Safety Software Framework version 1.0.1 ". Thanks.

0 Kudos

2,331 Views
shuangjunzhu
NXP Employee
NXP Employee

In document "S32G_SAF_SBOOT_UM.PDF", chapter "7.4.2 Steps to generate the sBoot configuration using S32CT", it mentioned to download the "S32 SAF Update Site zip file".

 

Can you please let me known where I can get it?

 

Thanks,

Jeff

0 Kudos