S12ZVL128 FMEDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL128 FMEDA

1,454 Views
Stefan_73
Contributor I

Coverage of listed in the FMEDA template Safety Mechanisms seems to be unsatisfactory low in relation to ASIL targets (max 20% in Flash FMEDA). For now we only have one document: MC9S12ZVxSM which is missing a lot of Safety Mechanisms to which FMEDA files refers. Can you provide us full description of Safety Mechanisms listed in FMEDA files?

0 Kudos
3 Replies

1,437 Views
aarul
NXP Employee
NXP Employee

Hi

The main safety mechanism for Flash is ECC which has 99% Diagnostic coverage. The software based self-test gives low coverage on some blocks and so it is pessimistically claimed at 20%. Overall the metrics are still met.

I recommend to look at the Safety Analysis Reports along with the FMEDA for details on safety mechanisms. I see that currently it is not published on the site. Give us couple of days and we will get it updated.

Regards

-Aarul

0 Kudos

1,431 Views
Stefan_73
Contributor I

Thank you for the answer.

Do you know when approximately this Safety Analysis Report will be uploaded to NXP site? This issue is extremely urgent for us?

 

 

0 Kudos

1,420 Views
naveenm
NXP Employee
NXP Employee

Hi,

The reports are available. 

Please let us know if you face issues.

Regards,

NaveenM

0 Kudos