PLL LOCK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PLL LOCK

1,257件の閲覧回数
HeebeomPark
Contributor II

 

Once the safety manual is updated to 6.0, there is additional comment like below.

 

[Questions] What does it the aforementioned system level checks? It is more like E2E protection? If not, can you specify which system level safety measures shall be used?

 

HeebeomPark_0-1739182599494.png

 

0 件の賞賛
3 返答(返信)

1,116件の閲覧回数
antoinedubois
NXP Employee
NXP Employee

HI Heebeom,

Yes SM4 E2E protection is the mentionned safety measures. If clock is incorrect, it will result in corruption, or delayed covered by the SM4 E2E safety mecahnisms

0 件の賞賛

1,170件の閲覧回数
john_floros
NXP Employee
NXP Employee

Hello,

This is SM4 E2E protection and is a software safety mechanism, to be implemented by the system developer.

Regards,

John

0 件の賞賛

1,153件の閲覧回数
HeebeomPark
Contributor II

Back to my original question, only SM4 which is E2E is sufficient to cover what Safety Manual describes?

0 件の賞賛