NXP S32G FCCU Application Note

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP S32G FCCU Application Note

912件の閲覧回数
EmmanuelDoit
Contributor II

Dear NXP Safety experts, is there an Application Note for the FCCU on S32G2? Or please confirm if the application note for FCCU from another processor is valid for the S32G2? Note: I have found Application Note for FCCU on different processors (e.g. for the MPC574xP). 

タグ(2)
0 件の賞賛
1 返信

906件の閲覧回数
nxa11829
NXP Employee
NXP Employee

Hi Emmanuel,

 

No there is not an application note for the FCCU on S32G2. The main sources of information on the FCCU are: the FCCU chapter in the S32G2 RM, the Fault Map attachment to the RM (including the notes at the foot of the page) and the S32G2 safety manual.

Please let us know if there is a specific aspect of the FCCU that is not clear.

 

Many thanks,

Alison

0 件の賞賛