FS26 Safety manual verify OTP bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 Safety manual verify OTP bits

ソリューションへジャンプ
1,281件の閲覧回数
oskarjohansson
Contributor I

I'm going through the safety manual for FS26 and multiply "System Integration Requirement" that's about verifying the OTP bits. I have a predefined OTP configuration that are stated in the product datasheet ch. 25. 

Is it possible to read out the OTP registers over SPI like the main/fs registers or should you read the M_PROGID register and compare to the predefined OTP configuration name?

Best regards,

Oskar

0 件の賞賛
1 解決策
1,233件の閲覧回数
r40959
NXP Employee
NXP Employee

Hello Oskar,

hoping it can help:

 

For most of these SIR about OTP check, they are referring to the OTP creation process when a customer is building its own OTP creation, discussing back and forth with NXP through FAE. Once a device is programmed, OTP bits can only be read thanks to our GUI and the mirror registers not through SPI commands. The register M_PROGID can give you the OTP ID but not the details of the configuration itself. Anyway, since you’re using one of our standard OTP/part number, you are not concerned by these SIR from the safety manual.

 

Best regards

Valerie

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,234件の閲覧回数
r40959
NXP Employee
NXP Employee

Hello Oskar,

hoping it can help:

 

For most of these SIR about OTP check, they are referring to the OTP creation process when a customer is building its own OTP creation, discussing back and forth with NXP through FAE. Once a device is programmed, OTP bits can only be read thanks to our GUI and the mirror registers not through SPI commands. The register M_PROGID can give you the OTP ID but not the details of the configuration itself. Anyway, since you’re using one of our standard OTP/part number, you are not concerned by these SIR from the safety manual.

 

Best regards

Valerie

0 件の賞賛