AES EVICTION TIME

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AES EVICTION TIME

1,979 次查看
HeebeomPark
Contributor II

The following is an assumption requirement from safety manual 6.0 for 32k388.

for e), the application shall trigger timer or is there any dedicated timer for AES eviction?

HeebeomPark_1-1739278892596.png

 

 

0 项奖励
5 回复数

1,861 次查看
antoinedubois
NXP Employee
NXP Employee

The timer is built into the AES. In this context it is assumed for a failure mode that would result in an unacceptable delay. It may be use for security measure too, but I am not a security expert. You can probably check with security team and within security reference manual.

0 项奖励

1,841 次查看
HeebeomPark
Contributor II

Thanks. Where is the security dedicated document?

Also with the keyword "Eviction" , no word in the latest reference manual [S32K3XXRM_rev 8.pdf]. 

 

 

 

0 项奖励

1,682 次查看
john_floros
NXP Employee
NXP Employee

Heebeom,

I apologize for the delay on this.  This mention of the eviction timer needs to be removed from the S32K3 Safety Manual.  It is not part of the AES IP on the S32K3.

Regards,

John

0 项奖励

1,663 次查看
HeebeomPark
Contributor II

thank you very much!

0 项奖励

1,922 次查看
HeebeomPark
Contributor II

Additional question: What is the background of the eviction time to be considered? For which attack, the eviction timer is considered?

0 项奖励