AES EVICTION TIME

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AES EVICTION TIME

1,985件の閲覧回数
HeebeomPark
Contributor II

The following is an assumption requirement from safety manual 6.0 for 32k388.

for e), the application shall trigger timer or is there any dedicated timer for AES eviction?

HeebeomPark_1-1739278892596.png

 

 

0 件の賞賛
5 返答(返信)

1,867件の閲覧回数
antoinedubois
NXP Employee
NXP Employee

The timer is built into the AES. In this context it is assumed for a failure mode that would result in an unacceptable delay. It may be use for security measure too, but I am not a security expert. You can probably check with security team and within security reference manual.

0 件の賞賛

1,847件の閲覧回数
HeebeomPark
Contributor II

Thanks. Where is the security dedicated document?

Also with the keyword "Eviction" , no word in the latest reference manual [S32K3XXRM_rev 8.pdf]. 

 

 

 

0 件の賞賛

1,688件の閲覧回数
john_floros
NXP Employee
NXP Employee

Heebeom,

I apologize for the delay on this.  This mention of the eviction timer needs to be removed from the S32K3 Safety Manual.  It is not part of the AES IP on the S32K3.

Regards,

John

0 件の賞賛

1,669件の閲覧回数
HeebeomPark
Contributor II

thank you very much!

0 件の賞賛

1,928件の閲覧回数
HeebeomPark
Contributor II

Additional question: What is the background of the eviction time to be considered? For which attack, the eviction timer is considered?

0 件の賞賛