AES EVICTION TIME

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AES EVICTION TIME

1,958 Views
HeebeomPark
Contributor II

The following is an assumption requirement from safety manual 6.0 for 32k388.

for e), the application shall trigger timer or is there any dedicated timer for AES eviction?

HeebeomPark_1-1739278892596.png

 

 

0 Kudos
5 Replies

1,840 Views
antoinedubois
NXP Employee
NXP Employee

The timer is built into the AES. In this context it is assumed for a failure mode that would result in an unacceptable delay. It may be use for security measure too, but I am not a security expert. You can probably check with security team and within security reference manual.

0 Kudos

1,820 Views
HeebeomPark
Contributor II

Thanks. Where is the security dedicated document?

Also with the keyword "Eviction" , no word in the latest reference manual [S32K3XXRM_rev 8.pdf]. 

 

 

 

0 Kudos

1,661 Views
john_floros
NXP Employee
NXP Employee

Heebeom,

I apologize for the delay on this.  This mention of the eviction timer needs to be removed from the S32K3 Safety Manual.  It is not part of the AES IP on the S32K3.

Regards,

John

0 Kudos

1,642 Views
HeebeomPark
Contributor II

thank you very much!

0 Kudos

1,901 Views
HeebeomPark
Contributor II

Additional question: What is the background of the eviction time to be considered? For which attack, the eviction timer is considered?

0 Kudos