s32v234-evb sd-card image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32v234-evb sd-card image

2,072 Views
willcampo
Contributor III

Good morning.
I'm trying to create a bootable SD card for the S32V234 Evaluation Board.
But somehow I get the following error in Matlab:


"C: \ Users \ waclab \ Documents \ MATLAB \ Add-Ons \ Toolboxes \ NXP_Vision_Toolbox_for_S32V234 \ code \" \ internals \ target \ create \ "" nxpvt_create_target.exe "..path" is not recognized as an internal or external command,
program or batch file executable.

1 Reply

1,603 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi willcampo@hotmail.com‌,

Sorry for the long delay but we (MATLAB Tools team) do not track this community for issues. We have our own space here: NXP Model-Based Design Tools for VISION 

Anyhow, in case you have not solve the problem up to this point please consider:

  1. Add the ..\NXP_Vision_Toolbox_for_S32V234\code\internals\target\create\ folder manually to the MATLAB path using right click\Add To Path\Selected Folders and Subfolders. Ideally this should be done automatically by MATLAB during toolbox installation
  2. If this does not work, try to run the MATLAB nxpvt_create_target() directly from the folder indicated above. This way it should work for sure since the exe is in the same location as the script.

Please let us know if it worked.

... and for the future, please consider adding your questing directly into the Model-Based Design Tools for Vision community in order to ensure a faster response.

Thank you!

Daniel