prebuilt Linux images to boot the S32V234-EVB board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

prebuilt Linux images to boot the S32V234-EVB board?

1,966 次查看
m2sawyer
Contributor I

My company received two S32V234-EVB boards from NXP but they don't appear to have any linux OS or even uboot on them.  The best I could do is get partial serial communication working over the micro USB connector using 38400,7,E,1 baud settings.  Are there any prebuilt Linux images that I could flash on to an SD card to boot the board?

Thanks

Michael

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,499 次查看
bpe
NXP Employee
NXP Employee

NXP provides a Linux-based SDK for S32V development boards. The package installs on a Linux PC and can build binaries for your board from verified sources and with a verified toolchian/configuration. Please contact your distributor to obtain the package.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,499 次查看
bpe
NXP Employee
NXP Employee

Just checked what is actually available, there _are_ pre-built binaries, so you even to no t have to built them

on your machine. Just contact your distributor to help you to access the download page.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复