prebuilt Linux images to boot the S32V234-EVB board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

prebuilt Linux images to boot the S32V234-EVB board?

1,971件の閲覧回数
m2sawyer
Contributor I

My company received two S32V234-EVB boards from NXP but they don't appear to have any linux OS or even uboot on them.  The best I could do is get partial serial communication working over the micro USB connector using 38400,7,E,1 baud settings.  Are there any prebuilt Linux images that I could flash on to an SD card to boot the board?

Thanks

Michael

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,504件の閲覧回数
bpe
NXP Employee
NXP Employee

NXP provides a Linux-based SDK for S32V development boards. The package installs on a Linux PC and can build binaries for your board from verified sources and with a verified toolchian/configuration. Please contact your distributor to obtain the package.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,504件の閲覧回数
bpe
NXP Employee
NXP Employee

Just checked what is actually available, there _are_ pre-built binaries, so you even to no t have to built them

on your machine. Just contact your distributor to help you to access the download page.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信