emmc can't be formatted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emmc can't be formatted

2,754 Views
sybilmao
Contributor I

Hi,

We have developed a platform using S32V234 as the main controller, and have made many boards,among them there are some emmc can't be formatted. There is a 32G emmc(MTFC32GAKAEEF-AIT) per board. the process is, first run u-boot,then run nfsboot,I can login,then run fdisk,the partition table can be printed, the first partition starts at 2048 ends at 524287,Size 255M,Id c, Type W95 FAT32(LBA),and then run mkfs.vfat -n boot /dev/mmcblk0p1,it suspends.

I have tried to change the start position of the first partition and have checked the partition table has changed,but it still can't be formatted.

What can I do except change a new eMMC chip?

0 Kudos
Reply
1 Reply

2,448 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is howto document related to eMMC, but I'm not sure if it covers your issue ( not tested with SBC board ) . But you can try it - https://community.nxp.com/docs/DOC-340293 

Jiri

0 Kudos
Reply