S32V: SRC_GPR Registers: Write failures?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32V: SRC_GPR Registers: Write failures?

3,432 次查看
ektasachdev
Contributor II

Hi,

 

I'm trying to configure the PCIE related registers on the S32v EVB board and I keep encountering strange behaviour.

For example, once QNX is up and running on the S32V EVB board, I tried reading the SRC_GPR5 register (address: 0x4007C110). The read succeeded and I got the following value -- 0x12500208 .

 

However, if I try to write to this register after the OS has booted, I get a bus error.

 

I can easily configure this registers in IPL and u-boot. I can't seem to do it after QNX is up and running. I've checked that the register itself is R/W and is a non-secure register (based on the TRM).

 

Can someone let me know if the TRM was updated or there is anything special I need to do to write to these registers once the OS is up and running?

 

 


Thanks,

Ekta

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

3,258 次查看
KushalShahNXP
NXP Employee
NXP Employee

Hi Ekta,

From your question, it seems that it is some prevention mechanism in QNX OS that is preventing access to this register.

I will recommend to contact QNX for support.

Regards,

Kushal

0 项奖励
回复