S23V234 platform:the max current per power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S23V234 platform:the max current per power supply

5,920 Views
YMS_Yuanming_Shu
NXP Employee
NXP Employee

1.do you have the detail list that the max current per power supply about the s23v234 platfrom?because many customers request the detail table for deigning the product's power domain.

   the name of per power supply table is as below:

   VDD_DDR_IO/VDD_HV_DDR(1/2/3)/VDDIO_LFAST/VDD_HV_IO_ETH(1/2)/VDD_HV_IO_FLA/VDD_HV_IO_DIS(1/2/3)/VDD_HV_IO_VIU0(1/2)/VDD_HV_IO_VIU1/VDD_GPIO0/VDD_GPIO1/VDD_GPIO2/VDD_LV_POST

Labels (1)
0 Kudos
Reply
2 Replies

5,474 Views
tombrown
NXP Employee
NXP Employee

Hello Sym,

This forum is no longer active.

I will work with you offline on these questions.

Regards,

Tom

0 Kudos
Reply

5,474 Views
YMS_Yuanming_Shu
NXP Employee
NXP Employee

okay,thanks!

0 Kudos
Reply