INTEGRATE LLCE_CAN/LIN(MCAL DRIVER) TO S32DS 3.4 ,But S32 DS Bulid ERROR

cancel
Showing results for 
Search instead for 
Did you mean: 

INTEGRATE LLCE_CAN/LIN(MCAL DRIVER) TO S32DS 3.4 ,But S32 DS Bulid ERROR

891 Views
ChenXiang
Contributor I

Hello everyone,

        When I follow the document “INTEGRATE LLCE_CAN/LIN(MCAL  DRIVER) TO S32DS 3.4”,I have some problems。微信图片_20221104164901.png

      when i build the project,It wasn't as successful as the documentation。
      The error is shown below。

Description Resource Path Location Type
#error "MemMap.h, no valid memory mapping symbol defined." LLCE_CAN_LIN_M7_0 line 12754, external location: D:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203\Base_TS_T40D11M30I2R0\include\Ecum_MemMap.h C/C++ Problem
#error "MemMap.h, no valid memory mapping symbol defined." LLCE_CAN_LIN_M7_0 line 12754, external location: D:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203\Base_TS_T40D11M30I2R0\include\Rte_MemMap.h C/C++ Problem
#error "MemMap.h, no valid memory mapping symbol defined." LLCE_CAN_LIN_M7_0 line 12910, external location: D:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203\Base_TS_T40D11M30I2R0\include\Can_43_LLCE_MemMap.h C/C++ Problem
#error "MemMap.h, no valid memory mapping symbol defined." LLCE_CAN_LIN_M7_0 line 12910, external location: D:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03\SW32_RTD_4_4_3_0_2_D2203\Base_TS_T40D11M30I2R0\include\Lin_43_LLCE_MemMap.h C/C++ Problem
make: *** [llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:27: llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/Can_43_LLCE_Irq.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:27: llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/Can_43_LLCE.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:27: llce/plugins/Can_43_LLCE_TS_T40D11M10I0R0/src/Can_Llce.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/EcuM_TS_T40D11M10I0R0/src/subdir.mk:20: llce/plugins/EcuM_TS_T40D11M10I0R0/src/EcuM.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:26: llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/Lin_43_LLCE.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:26: llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/Lin_Llce_Irq.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/subdir.mk:26: llce/plugins/Lin_43_LLCE_TS_T40D11M10I0R0/src/Lin_Llce.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [llce/plugins/Rte_TS_T40D11M10I0R0/src/subdir.mk:20: llce/plugins/Rte_TS_T40D11M10I0R0/src/SchM_Can_43_LLCE.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** [src/subdir.mk:20: src/main.o] Error 1 LLCE_CAN_LIN_M7_0 C/C++ Problem
make: *** Waiting for unfinished jobs.... LLCE_CAN_LIN_M7_0 C/C++ Problem
'Linflexd_Uart_Ip_pHwConfigPB_0_BOARD_INITPERIPHERALS' undeclared (first use in this function); did you mean 'Linflexd_Uart_Ip_xHwConfigPB_0_BOARD_INITPERIPHERALS'? main.c /LLCE_CAN_LIN_M7_0/src line 296 C/C++ Problem。

微信图片_20221104165433.png

Can you give me some advice?Thanks!

0 Kudos
Reply
0 Replies