using MCSPTE1AK344_BLDC_6step_sensorless_II without GD3000 driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using MCSPTE1AK344_BLDC_6step_sensorless_II without GD3000 driver

871件の閲覧回数
Eduardo2000
Contributor I

We are using the NXP motor controller code  ( MCSPTE1AK344_BLDC_6step_sensorless_II ) and tested it on the NXP eval board which works well. We are now going to test the firmware on our own motor driver with same pinout as NXP eval board except that we are not using SPI based GD3000 driver.And instead, we use three regular non-spi drivers to drive the FETs. Can you let us know what   sections in the code need to be changed to remove the GD3000 part and still use the NXP code? As mentioned, everything else is the same! Appreciate your urgent response. 

0 件の賞賛
返信
1 返信

813件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

We do not have an app note for Six-Step Commutation Control like we have for Field-Oriented Control, nor do we have an example for a non-SPI gate driver. An apology for the inconvenience.

However you could refer to S32K344 - Six-step commutation control and also to 4. Software implementation on the S32K344 section from AN13767, which is a demo with similar Software Architecture.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信