uja1076 wake up event via can message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uja1076 wake up event via can message

401 Views
maximillion
Contributor II

Hi @TomasVaverka 

I will try to wake SBC with the CAN message mentioned in your application note. "The UJA107XA requires a wake-up sequence consisting of recessive, dominant, recessive, dominant signal on the CAN bus within the specified tto(wake) time. So each phase should be 0.5…3us (tbus(rec)(min)) , tbus(dom) ) )(min)).
Should I send 4 bytes of data [0x01,0x00,0x01,0x00] created according to this paragraph?
Also, can you give detailed information about the phase timing?
Should the time to send 1 byte data be between 0.5…3us?
I will use S32K148 EVB to send wake up message. Should I use the bitrate configuration of the flexcan module to perform the specified time? Could you share bit configuration value

0 Kudos
Reply
0 Replies