the PWM output frequency issue on S32K3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

the PWM output frequency issue on S32K3

跳至解决方案
2,688 次查看
zp001
Contributor III

Hello,

There is a problem about PWM output frequency, the configuration of PWM is as below:

eMIOS_Mcl configuration:

  1. eMIOS_0 source clock is 160Mhz
  2. eMIOS_0 clock divider is 200 and the default period is 65535

PWM channel configuration:

  1. clock prescaler is DIV_1
  2. prescaler clock source is EMIOS_PWM_SRC_PRESCALED_CLOCK
  3. the period is 65534

the frequency of this channel should be calculated by below formula:

output frequency = 160000000 / 200 / 65534 = 12.2Hz

but I got a 3.67hz waveform.

zp001_0-1671187280380.jpeg

It looks like the source clock divided by 3 once again.

I have double checked the configurations and can't find any clue.

I'd like to know why this phenomenon should occur.

RTD is 2.0.1 

S32DS V3.5

Thanks!

 

标记 (1)
0 项奖励
回复
1 解答
2,669 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

your calculation is correct, but in your project the core clock is running from FIRC, not the PLL. This makes that difference. 
For clock init use below function

/* Initialize clock */
Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,670 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

your calculation is correct, but in your project the core clock is running from FIRC, not the PLL. This makes that difference. 
For clock init use below function

/* Initialize clock */
Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);

BR, Petr

0 项奖励
回复
2,671 次查看
zp001
Contributor III

Hello,

I tried to read PLL clock via Clock_Ip_GetFreq(PLL_CLK);

The PLL clock is zero, that is inconsistent with the clock map.

标记 (1)
0 项奖励
回复