Hi,
I encountered a clock issue on the S32K358 development board, When I set the PLL0 to a 240MHz clock, the chip could not be programmed. However, when I set the PLL0 to a 160MHz clock, the chip worked normally. Is there any resolution for this issue?
Thanks & BR.
Hi @wenhui,
What do you mean it can't be programmed?
Programmed by a JTAG/SWD programmer or by the application via the flash controller?
Is the HSE_FW installed?
Regards,
Daniel