s32k358 SBC voltage monitoring

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k358 SBC voltage monitoring

1,376 Views
mariam
Contributor I

I need an example of SBC voltage monitoring for s32k388??
and want to ask why in s32k388 example enabled the Vmon reactions and the FCCU monitoring disabled ??

0 Kudos
Reply
4 Replies

1,317 Views
CongDang
NXP Employee
NXP Employee

S32K388 example: Plan End of December

FCCU Monitoring enables or disable depend by user.

You can enable to monitor. Need to take care the signal of fault at FCCU1/2 when enable FCCU.

0 Kudos
Reply

1,312 Views
MarinaMagdy
Contributor I

Hi CongDang,

Thanks for your support.
When to choose PAIR, Single and FCCU1/2 what is the difference between these options? 

FCCU CFG.png

0 Kudos
Reply

1,301 Views
CongDang
NXP Employee
NXP Employee

Data sheet of SCB should help for more detail.

CongDang_0-1699423303182.png

 

0 Kudos
Reply

1,340 Views
MarinaMagdy
Contributor I

Any updates??

0 Kudos
Reply