s32k312 basic secure boot workflow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k312 basic secure boot workflow

2,276件の閲覧回数
fantong9
Contributor I

pls help me to check if understand correct?

1. for hse basic secure boot,  the app integrity check is by bootloader,   so it need a additional software (bootloader ) to do it.  bootloader maybe a normal app and not started with secure boot, so it may be modified and app cant be fully trusted.

2. in HSE demoExample-Advanced_secure_boot project, it just run once to setup the SMR data. after reset, it can be erased and hse firmware check the smr data and jump to the app if passed check.

0 件の賞賛
返信
1 返信

2,215件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @fantong9 

To better understand the Secure Boot we provide an application note including demo projects which explains all the steps in detail. It can be downloaded from:
S32K3 Microcontrollers for Automotive General Purpose

Application note can be found here:
Documentation -> Secure Files -> Secure Boot Application note v0.1.1.0 (AN744511)

Associated demo project can be downloaded here:
Design Resources -> Software -> Secure Files -> SecureBootAppNoteDemo (SW745310)

 

BR, VaneB

0 件の賞賛
返信